Peripheral device disconnects when performing parameter update with latency 420
Hogp device requests to pair again with iPhone 6s
Cscp collector crashes during sending notifications and scanning (Malloc failure)
Cscp collector crashes during sending notifications and scanning (CMAC error)
RSSI reading in LP mode have 2dB error
eFlash read error in Cli_Programmer Tool
Xtal 32kHz may fail to start up at low temperature
Read BD address from CS not working
Transmit power levels in the SDK are not on par with the datasheet.
Configuration Script is overwritten with new firmware
Compiler error when SDADC is used without DMA
Asymmetric SUOTA application does not support GAP security level 3
Sometimes SUOTA requests a new passkey after one or more attempts
Update asymmetric SUOTA when application software updates to a new version
Update both asymmetric SUOTA and application software when keys are revoked
Python script ‘program_nvparam’ returns with error
Revision History
DA1459x SDK Known Limitations List
Search
Please activate JavaScript to enable the search functionality.