Cscp collector crashes during sending notifications and scanning (CMAC error)

ID: DA1459xSDK-736

Status: Open

First reported: 10.1.2.86

Fixed in: TBD

Description

Cscp collector application in the SDK fails (crashes) after about 1 hour when paired and bonded with an iPhone SE while scanning for cadence and/or speed sensors. So far this issue has been observed only with iPhone SE (iOS version 15.1). The application crashes with a CMAC error.

Workaround

At this moment there is no workaround available.