Hogp device requests to pair again with iPhone 6s
ID: DA1459xSDK-732
Status: Open
First reported: 10.1.2.86
Fixed in: TBD
Description
Hogp device requests to pair again with iPhone 6S after phone’s Bluetooth is turned off/on. This issue was observed only with iPhone 6S and with no other iOS devices nor with Android devices.
Workaround
There is no workaround, iPhone 6S needs to re-pair again.