Update asymmetric SUOTA when application software updates to a new version

ID: DA1459xSDK-972

Status: Open

First reported: 10.1.6.108

Fixed in: TBD

Description

When version numbering is used to prevent image roll-back and the version number and minimal version number of the application software is higher than the asymmetric SUOTA version number, then the application software can never be updated anymore since asymmetric SUOTA version < application version.

Workaround

When updating the application software with an increased version- and minimal version number then first the asymmetric SUOTA needs to be updated with an increased version number.