Peripheral device disconnects when performing parameter update with latency 420
ID: DA1459xSDK-726
Status: Open
First reported: 10.1.2.86
Fixed in: TBD
Description
When the slave latency is set to 420, the peripheral device gets disconnected when a parameter update is executed.
Workaround
Set slave latency < 420.