eFlash read error in Cli_Programmer Tool

ID: DA1459xSDK-761

Status: Fixed

First reported: 10.1.2.86

Fixed in: 10.1.4.104

Description

Reading the content of the eFlash of the DA14592 SOC using the Segger GDB Server may result in erroneous read results. The read error has not been encountered when the read_eflash command is used over the UART.

Workaround

A fixed version of the Cli_programmer.exe tool (Windows) can be downloaded from: https://lpccs-docs.renesas.com/DA14592_Cli_Programmer/cli_programmer.zip