Cscp collector crashes during sending notifications and scanning (Malloc failure)

ID: DA1459xSDK-735

Status: Fixed

First reported: 10.1.2.86

Fixed in: 10.1.4.104

Description

Cscp collector application in the SDK fails (crashes) after about 1 hour when paired and bonded with an iPhone SE while scanning for cadence and/or speed sensors. So far this issue has been observed only with iPhone SE (iOS version 15.1). The application crashes with a MallocFailed error.

Workaround

At this moment there is no workaround available.