Configuration Script is overwritten with new firmware
ID: DA1459xSDK-893
Status: Fixed
First reported: 10.1.2.86
Fixed in: 10.1.6.108
Description
When a new firmware is programmed in the eFlash using e2Studio, the Configuration Script is overwritten whith new values.
This especially jeopardize the DA14592 Module as the Configuration Script is pre-programmed whith a Crystal Trim Value.
Workaround
Before programming a new firmware into the DA14592 Module, read out the Configuration Script using either the SmartSnippets Toolbox or Cli_programmer and store the value for later use.