Logo
  • Unencrypted PDU’s allowed during secure connection pairing after LL_ENC_REQ from master.
  • The cscp_collector disconnects with reason code 0x3d when using an iPhone 16 as the peripheral device
  • Controller does not apply MinCI != MaxCI in LL_CONNECTION_PARAMETER_REQ when in Master role
  • Assertion Crash in cscp_collector during concurrent BLE scanning and notification handling
  • DA1469x accepts invalid Static Random Address
  • Secure Connections not implemented in ble_suota_client application
  • PXP_Reporter with encryption may have lower throughput using SUOTA with Android versions 15 and 16
  • Skip Slave Latency (via SDK API Call) does not work
  • Whitelist support not present in BLE Manager of SDK10
  • Starting undirected advertising with a Random Non-Resolvable Private Address returns Error
  • Revision History
DA1469x SDK Known Limitations List
  • Search


© Copyright 2025, Renesas Electronics Corporation.