Secure Connections not implemented in ble_suota_client application
ID: DA1469xSDK-4048
Status: Open
First reported: 10.0.12
Fixed in: TBD
Description
The ble_suota_client application has no Security Level 3 implemented out-of-the-box and therefore fails to establish a secure connection with the pxp_reporter (SUOTA) application when security is enabled.
Workaround
Secure connections in the ble_suota_client can be added by implementing Security Level 3 in the application.