Skip Slave Latency (via SDK API Call) does not work

ID: DA1469xSDK-4052

Status: Open

First reported: 10.0.12

Fixed in: TBD

Description

When enabling the Skip Slave latency API and using the function ble_gap_skip_latency( ) , no effect is observed in a connection with latency

Workaround

At this moment there is no workaround available.