DA1469x accepts invalid Static Random Address
ID: DA1469xSDK-4046
Status: Open
First reported: 10.0.12
Fixed in: TBD
Description
DA1469x accepts invalid static address ( 0x FFFFFFFFFFFF, the 2 most significant bits set to ‘1’ )
Workaround
Be sure that BD address 0xFFFFFFFFFFFF and 0xC00000000000 cannot be set as valid static random address.