Unencrypted PDU’s allowed during secure connection pairing after LL_ENC_REQ from master.
ID: DA1469xSDK-4038
Status: Open
First reported: 10.0.12
Fixed in: TBD
Description
When in Secure Connection Pairing , the controller of the DA1469x (Peripheral) , allows reception of unencrypted SM PDUs from master after LL_ENC_REQ until the secure connection is complete. The unencrypted PDU’s will never be handled by the application and therefore are not a security issue. When in Legacy pairing, controller correctly abandons the connection with a MIC error when this happens.
Workaround
At this moment there is no workaround available.