PXP_Reporter with encryption may have lower throughput using SUOTA with Android versions 15 and 16
ID: DA1469xSDK-4051
Status: Open
First reported: 10.0.16
Fixed in: TBD
Description
The pxp_Reporter with encryption has lower throughput using SUOTA with Android versions 15 and 16. The pxp_Reporter without encryption has the expected throughput.
Workaround
For Suota enabled pxp_Reporter, the connection interval needs to be changed to a shorter time.