Starting undirected advertising with a Random Non-Resolvable Private Address returns Error
ID: DA1469xSDK-4055
Status: Open
First reported: 10.0.12
Fixed in: TBD
Description
When Random Non-Resolvable Private Address is set, connectable advertising fails to start when calling ble_gap_adv_start(GAP_CONN_MODE_UNDIRECTED).
Workaround
Use non connectable mode (GAP_CONN_MODE_NON_CONN)