The cscp_collector disconnects with reason code 0x3d when using an iPhone 16 as the peripheral device
ID: DA1469xSDK-4039
Status: Open
First reported: 10.0.16
Fixed in: TBD
Description
cscp_collector disconnects after some time with reason 0x3d when use iphone 16 as a peripheral device. The disconnect time can vary between 30 minutes and several hours.
Workaround
At this moment there is no workaround available.