Assertion Crash in cscp_collector during concurrent BLE scanning and notification handling
ID: DA1469xSDK-4044
Status: Open
First reported: 10.0.12
Fixed in: TBD
Description
The cscp_collector application crashes with an assertion failure inside ad_uart_read_async when scanning is re-initiated while notifications are being received.
Workaround
At this moment there is no workaround available.