Controller does not apply MinCI != MaxCI in LL_CONNECTION_PARAMETER_REQ when in Master role

ID: DA1469xSDK-4040

Status: Open

First reported: 10.0.12

Fixed in: TBD

Description

When issuing a Connection Update Command with MinCI != MaxCI from Host , Controller outputs minCI = maxCI PDU when in Master Role. When in Slave Role , then it correctly outputs MinCI != MaxCI.

Workaround

At this moment there is no workaround available.