Unencrypted PDU’s allowed during secure connection pairing after LL_ENC_REQ from master.
The cscp_collector disconnects with reason code 0x3d when using an iPhone 16 as the peripheral device
Controller does not apply MinCI != MaxCI in LL_CONNECTION_PARAMETER_REQ when in Master role
Assertion Crash in cscp_collector during concurrent BLE scanning and notification handling
DA1469x accepts invalid Static Random Address
Secure Connections not implemented in ble_suota_client application
PXP_Reporter with encryption may have lower throughput using SUOTA with Android versions 15 and 16
Skip Slave Latency (via SDK API Call) does not work
Whitelist support not present in BLE Manager of SDK10
Starting undirected advertising with a Random Non-Resolvable Private Address returns Error
Revision History
DA1469x SDK Known Limitations List
Index
Index