This section describes how to quickly get started with the DA14535 TINY™ Module with Devkit-p and run the pre-loaded demo.
Please be aware that there is an issue in the ble_app_all_in_one project within the SDK. Please refer to this SDK6 Known issue for more details.
Make sure that you have all required tools installed as described in Section 5 and Section 6.
Then Open SmartBond application on your Smart phone and toggle Scan on the right top side of the screen. You Should find “SUoutA_only” on your device list like the figure below:
By viewing this on your device list , simply you see a ble application advertising and your device works as expected.
SmartBoot
SmartBoot is a web based tool where we create an image with the a specific memory layout with the secondary bootloader that can optionally be used to add functionality to the boot sequence of DA14535 and DA14535MOD devices. The features added by the SmartBoot bootloader include two wire uart booting and enabling Software Updates over the Air (SUotA).
We strongly recommend that you visit SmartBoot for more information.
This tutorial does not cover all the topics relevant to software development environments, it describes the first steps necessary
to get started with the DA14535 TINY™ Module. The following links provide more information on DA14535:
AN-B-098 DA14535 Hardware guidelines : To learn more about schematic, circuit explanation, and design guidelines for BLE applications based on the DA14535 SoC.