7. RF Testing Unit (RFTU)
7.1. Selection
Different RFTU’s can be used in combination with the Connectivity Production Line Tool. Which RFTU to select depends on the target protocol for wireless testing. The available RFTU’s are listed in Table 1
Protocol |
Devkit |
Link |
Additional info |
|---|---|---|---|
Bluetooth LE |
DA14695 USB Kit |
7.2. BLE RFTU
For testing Bluetooth LE applications, Renesas Electronics Coorporation offers the DA14695 USB Kit with RFTU software as a ready to use RF testing solution. The hardware of this RFTU is exactly the same as the standard DA14695 USB Kit, but the RFTU software is preloaded. Instructions for flashing the DA14695 USB Kit with RFTU software can be found in the following section.
7.2.1. Flashing DA14695 USB Kit RFTU
To flash the RFTU software to the DA14695 USB Kit, a flash programmer and the RFTU software binary is needed. The software binary is included with the Connectivity Production Line Tool release package. And as the flash programmer, Renesas Electronics Coorporation SmartSnippets™ Toolbox is recommended. The steps to flash the software are as follows.
Locate the software in the Connectivity Production Line Tool release package at
C:\Renesas Electronics\Renesas Connectivity PLT\Firmware\Rftu\DA14695-00HQDEVKT-U\st_fw.binDownload Renesas Electronics Coorporation SmartSnippets™ Toolbox from SmartBond Development Tools Product Page
Run the installer
Start SmartSnippets™ Toolbox
Plug in the DA14695 USB Kit, and verify the dip switch settings (Figure 24)
Figure 24 DA14695 USB Kit dip switch settings
Select the device
Figure 25 SmartSnippets™ Toolbox device selection
Select the UART
Figure 26 SmartSnippets™ Toolbox COM selection
Open the programmer
Figure 27 SmartSnippets™ Toolbox flash programmer
Click import from file
Figure 28 SmartSnippets™ Toolbox import from file
Select binary file from the PLT release package
C:\Renesas Electronics\Renesas Connectivity PLT\Firmware\Rftu\DA14695-00HQDEVKT-U\st_fw.binFigure 29 SmartSnippets™ Toolbox select binary file
Click prepare image
Figure 30 SmartSnippets™ Toolbox prepare image
Click OK
Figure 31 SmartSnippets™ Toolbox ok prepare image
Click Connect (Figure 32), and if the logs ask to press the reset, press reset button (K2, Figure 33)
Click Read (this will fill the flash size which is needed before programming)
Figure 34 SmartSnippets™ Toolbox read flash
Finally, click Burn to program the flash
Figure 35 SmartSnippets™ Toolbox burn flash