Quick Start
Refer to the Hardware Setup to setup the jumpers on your development kit.
Call:
pip install py-ble-manager[dev]to install thepy_ble_managerpackage and its dependencies.Note
Specifying [dev] will install optional dependency: prompt_toolkit.
prompt_toolkitis used in some of the examples to provide a command line interface.Note
This library requires Python v3.10.5 or later.
Note
It is recommended to install the library using a virtual environment. To setup a virtual environment using venv call: $ python -m venv ./<name_of_your_env>. Note to create a virtual environment that uses Python 3.10.5, you must already have Python 3.10.5 downloaded on your computer. To use the above command to create a Python 3.10.5 environment, Python 3.10.5 must be configured in your PATH. You can download it from the python website.
Download the py_ble_manager enabled firmware binary to the development kit by calling the
py_ble_manager_programmerutility from the terminal.The package is now installed and you are ready to run one of the examples!