Basic Usage
The primary interface to the library is the BleCentral class, which provides methods to initiate BLE operations
and handle asynchronous BLE events.
Create a BLE Central object and perform initialization
import py_ble_manager as ble
central = ble.BleCentral("COM54")
# Initialize the Python BLE Framework
central.init()
# Start operating as a BLE Central
central.start()
# Set the IO capabilities
central.set_io_cap(ble.GAP_IO_CAPABILITIES.GAP_IO_CAP_KEYBOARD_DISP)
Initiate a BLE Operation
Scanning
central.scan_start(type=ble.GAP_SCAN_TYPE.GAP_SCAN_ACTIVE,
mode=ble.GAP_SCAN_MODE.GAP_SCAN_GEN_DISC_MODE,
interval_ms=100,
window_ms=50,
filt_wlist=False,
filt_dupl=True)
Connecting
peripheral_addr: ble.BdAddress = ble.BleUtils.str_to_bd_addr("48:23:35:00:1b:53,P")
connection_params = ble.GapConnParams(interval_min_ms=50, interval_max_ms=70, slave_latency=0, sup_timeout_ms=420)
central.connect(peripheral_addr, connection_params)
Read a characteristic value
central.read(conn_idx=0, handle=24, offset=0)
Write a characteristic value
central.write(conn_idx=0, handle=24, offset=0, value=1234)
Disconnect
central.disconnect(conn_idx=0)
Handle asynchronous events
The framework returns asynchronous events to the application through an event queue. Calling BleCentral.get_event() will get an event from the queue.
All of the events returned by BleCentral.get_event() are a subclass of BleEventBase.
A variety of different events occur throughout the life a BLE application. Some example events include
BleEventGapConnectionCompleted, BleEventGapDisconnected,
BleEventGattcReadCompleted, BleEventGattcWriteCompleted.
Each event has an evt_code to identify the type of event.
For example, after you initiate a write you will receive a BleEventGattcWriteCompleted event which has an evt_code of
BLE_EVT_GATTC_WRITE_COMPLETED. Your application can
handle the event however it sees fit. If your application does not handle the event, call BleCentral.handle_event_default() to have the BLE framework process the event for you.
# This call will block until an event is available. Use the timeout parameter to block for a specified period of time
evt = central.get_event()
# Determine which event occurred. It will be of type BLE_EVT_GAP, BLE_EVT_GATTC, or BLE_EVT_GATTS
match evt.evt_code:
# Handle the event
case ble.BLE_EVT_GAP.BLE_EVT_GAP_ADV_REPORT:
# Define your own handling function to process the event
handle_evt_gap_adv_report(evt)
case ble.BLE_EVT_GAP.BLE_EVT_GAP_SCAN_COMPLETED:
handle_evt_gap_scan_completed(evt)
case ble.BLE_EVT_GAP.BLE_EVT_GAP_CONNECTED:
handle_evt_gap_connected(evt)
case ble.BLE_EVT_GAP.BLE_EVT_GAP_CONNECTION_COMPLETED:
handle_evt_gap_connection_completed(evt)
case ble.BLE_EVT_GAP.BLE_EVT_GAP_DISCONNECTED:
handle_evt_gap_disconnected(evt)
case ble.BLE_EVT_GATTC.BLE_EVT_GATTC_BROWSE_SVC:
handle_evt_gattc_browse_svc(evt)
case ble.BLE_EVT_GATTC.BLE_EVT_GATTC_BROWSE_COMPLETED:
handle_evt_gattc_browse_completed(evt)
case ble.BLE_EVT_GATTC.BLE_EVT_GATTC_NOTIFICATION:
handle_evt_gattc_notification(evt)
case ble.BLE_EVT_GATTC.BLE_EVT_GATTC_WRITE_COMPLETED:
handle_evt_gattc_write_completed(evt)
case ble.BLE_EVT_GATTC.BLE_EVT_GATTC_READ_COMPLETED:
handle_evt_gattc_read_completed(evt)
case _:
# For any events not handled by your application, call the BleCentral default handler to process the event
central.handle_event_default(evt)