Welcome to py_ble_manager’s documentation!
A python library for controlling Renesas BLE devices.
Purpose
The intent of this library is to provide a python interface similar to SDK10 for controlling BLE of DA14xxx devices. This is achieved by communicating with a development kit running Generic Transport Layer (GTL) supported firmware over a USB port on your PC:
The primary intent is for use as a central device for benchtop testing, continuous integration, or as an end-of-line tool. For additional information on the GTL please see the GTL User Manual