Source code for py_ble_manager.ble_api.BleCommonApi

from typing import Tuple
from ..ble_api.BleApiBase import BleApiBase
from ..ble_api.BleCommon import BLE_ERROR
from ..ble_api.BleConfig import BleConfigDefault
from ..manager.BleManager import BleManager
from ..manager.BleManagerCommonMsgs import BleMgrCommonResetCmd, BleMgrCommonResetRsp, BleMgrCommonGetDevVersionCmd, BleMgrCommonGetDevVersionRsp


[docs]class BleCommonApi(BleApiBase): def __init__(self, ble_manager: BleManager): super().__init__(ble_manager)
[docs] def ble_reset(self) -> BLE_ERROR: command = BleMgrCommonResetCmd() response: BleMgrCommonResetRsp = self._ble_manager.cmd_execute(command, 5) # timeout after 5 seconds if not response: raise TimeoutError("Failed to reset BLE stack. Check your development kit hardware setup" " and confirm the development kit is programmed with py_ble_manager firmware") return response.status
[docs] def get_dev_version(self) -> Tuple[BleConfigDefault, BLE_ERROR]: command = BleMgrCommonGetDevVersionCmd() response: BleMgrCommonGetDevVersionRsp = self._ble_manager.cmd_execute(command) return response.config, response.status