2. Abstract

This getting started guide describes how to build and run a sample application using e² studio. It shows step by step how to import an existing SDK 6 project into e2 studio and run it on an DA145xx Dev kit.

Renesas offers a variety of development kits for the DA14535, DA14531-00, DA14531-01 and DA14585/6 Bluetooth® devices. In this tutorial we will be using one of the following development kits:

Hint

  • This document is applicable to SDK6 (DA14585/6 and DA1453x)

  • DA1453x is referring to DA14531-00, DA14531-01, DA14530, DA14533 and DA14535.

  • DA1458x is referring to DA14585 and DA14586.

Here is a list of all hardware combinations supported by SDK6 and e2 Studio:

  • DA14531-00FXDEVKT-P Pro Motherboard (supports both DA1453x and DA1458x devices) with:

    • DA14530-00 daughterboard

    • DA14531-00 daughterboard

    • DA14531-01 daughterboard

    • DA14531MOD daughterboard

    • DA14535 daughterboard

    • DA14535MOD daughterboard

    • DA14533 daughterboard

    • DA1458x daughterboard

  • DA14535-00FXDEVKT-P Pro Motherboard (supports ONLY DA1453x devices) with:

    • DA14531-00FXDEVKT-P Pro Motherboard with:

    • DA14530-00 daughterboard

    • DA14531-00 daughterboard

    • DA14531-01 daughterboard

    • DA14531MOD daughterboard

    • DA14535 daughterboard

    • DA14535MOD daughterboard

    • DA14533 daughterboard