1. Prerequisites

To start building a fully working solution on e2 studio and SDK6 the following tools are being used:

  • Hardware tools:

    • Windows based PC

    • One of the Renesas development kit for the DA14535, DA14531-00, DA14531-01, DA14533 and DA14585/6 Bluetooth® devices

  • Software tools:

    • Download the latest SDK version for DA1453x and DA14585/DA14586

    • e2 studio 2025-12 or later

Note

You can refer to this video for how to install e2 studio.