DA14533 Getting Started with the Pro-Development Kits

R19US0026EE0100

DA14533 Arm® Cortex® M0+ is a member of the DA1453x family of Bluetooth® Low Energy (BLE) devices, which operates at Ultra-low power levels while delivering top-notch RF performance. This tutorial will guide you to gain an understanding about the hardware and walk you through building and running your first DA14533 application by Keil®.

The DA14533 is optimized for automotive and industrial applications at higher temperatures, and it is rated as operating up to 105 ºC and compliant with the AEC-Q100 (Grade 2) standard.

Note

DA1453x here is referring to:

  • DA14531-00

  • DA14531-01

  • DA14530

  • DA14535

  • DA14533.

Contents