2. Prerequisites
To start the evaluation or project development on Renesas DA14533 product sets, the following tools are being used here however the process is same with other development kit:
- Hardware tools:
Computational workstation (for example, PC or Laptop)
32-bit or 64-bit processor with 1 GHz processing speed
1 GB RAM
2 GB free disk space
DA14533-00FXDEVKT-P as a motherboard
USB cable for power supply to the Pro Development kit and for on-board debugging
- Software tools:
Terminal software such as RealTerm, Putty, or Tera Term. This document uses Tera Term for its examples
SmartSnippets™ Toolbox or later, which can be installed on Windows
Hint
When SmartSnippets™ is installed, all the sub-component drivers and software tools needed for DA14533 development are also installed.
- Bluetooth® explorer tool:
Type chrome://bluetooth-internals/#devices into the address field of the Chrome Browser to use the built-in tool (PC with Win10 or MAC book) or scan the QR code below based on your operating system
- Renesas Smartbond for IOS:
Use the QR code below
Figure 1 Scan the QR Code to install Renesas SmartBond for iOS
Or
- Renesas Smartbond for Android:
Use the QR code below
Figure 2 Scan the QR Code to install Renesas SmartBond for Android