4. The Hardware

The DA14533 Development Kit box consists of a DA1453x DEVKT-P Motherboard and a DA14533 Daughterboard featuring the DA14533 SoC of the desired package WFFCQFN22.

4.1. The DEVKT-P Motherboard

The motherboard provides the necessary hardware to enable:

  • Full digital connectivity with external hardware using UART, SPI, GPIO, and I2C

  • USB-based debugging capabilities using the SEGGER J-Link on-board debugger

  • USB-based UART communication with the host PC using a Future Technology Devices International (FTDI) chipset that converts UART to USB signal.

Which daughterboards are supported?

All daughterboards of the DA1453x family are compatible with the DA14531 DEVKT-P Motherboard. This motherboard has now been superseded with the new model DA1453x DEVKT-P Motherboard. The main difference is the new and more accurate power measurement circuitry. When you order DA14533 Development Kit, the new motherboard is shipped by default.

Note

The schematic diagrams, BOM, and Gerber files are illustrated in detail in the DA1453x DEVKT-P Motherboard.

Figure 5 shows the DA14533 daughterboard connected to the DA1453x DEVKIT-P Motherboard.

../_images/DA14533_Pro_Kit.svg

Figure 5 DA1453x DEVKIT-P layout

Note

The schematic diagrams, BOM, and Gerber files are illustrated in detail in the Development Kit Documentation.

4.2. What is new on DA1453x DEVKT-P Motherboard:

The DA1453x development box includes a Power Measurement Module (see J7 in Figure 11). PMM2 is an external add-on board that connects to the DEVKIT-P Motherboard via connector J7. This module offers a range of features, including:

  • A full-scale measurement range of 500 mA at 3.3 V

  • High-precision measurements down to 1 uA.

Another significant difference between the DA14531 and DA1453x DEVKIT-P Motherboard is the debugger. In the DA1453x DEVKIT-P Motherboard, the debugger U25 has been replaced with RA4M2. Additionally, it is worth noting that Mikrobus1, which was previously found on the DA14531 DEVKIT-P Motherboard, is no longer included in the DA1453x DEVKIT-P Motherboard. This change is due to the incompatibility between this motherboard and DA1458x family.

4.3. The Daughterboard

Figure 8 shows the DA14533 daughterboard.

../_images/Daughterboard33.svg

Figure 8 The DA14533 daughterboard

Winbond flash

The DA14533 daughterboard has an embedded 2 Mbit Winbond (W25X20CVUXSG) flash.

Power Mode Selection

The Power mode selection should be done on J4 on DA1453x DEVKIT-P Motherboard considering the jumper structure printed on the motherboard, see Figure 11. Make sure to configure this jumper for BUCK mode while downloading the program. Note that the J4 configuration has been made by default for BUCK mode and this note is only related to downloading step.

R-Multiplexer

The DA14533 daughterboards come with a default resistors (R-Multiplexer) configuration. This is a group of 16 resistors of 0 Ω that can be placed/removed in order to hardwire various peripherals to the DA14533 pins (from J1 or J2 ) as desired.

Extra Guideline

DA14533 Requirements for Spurious Reduction Application Note contains guidelines to implement a RFIO filter that serves to reduce conducted and radiated spurious emissions in Bluetooth® low energy applications.

4.4. Configure the DEVKIT-P Motherboard with Jumper Settings

Figure 11 shows the layout of the headers and its descriptions on the DA1453x DEVKIT-P Motherboard in Table 1.

../_images/jumper_Setting_535.svg

Figure 11 DA1453x DEVKIT-P Motherboard jumpers description

Table 2 DA1453x Motherboard elements

Jumper

Description

J1

Configuration header. SPI data flash, UART modes, JTAG, and Reset functions are enabled

J2

GPIO Break out header

J24

Software trigger

J8

T_RST (reset from J-Link), LED

J19

Enable user push buttons, SW2 and SW3

J9

Enable current sense circuit. Also, it allows the simultaneous connection of an external current measurement instrument

J5

VLDO output voltage selection

J4

DCDC Configuration: select either Boost, Buck, or Bypass mode

J7

Current measurement Socket

J23

Reset options

Warning

Do not remove J8 jumper. The J8 (pin 1-2) is no longer an user jumper (J8 is the reset sourced from RA4M2). Removing this jumper will cause the J-link reset to be high always, considering this point and placing J23 (pin 2-3) will cause VLDO to be cut from the daughterboard.

Figure 12 shows the layout of the header J1 in DA1453x development board.

../_images/j1layout.svg

Figure 12 The DA1453x DEVKIT-P Motherboard J1 layout

Warning

Do not remove J8 jumper. The J8 (pin 1-2) is no longer an user jumper (J8 is the reset sourced from RA4M2). Removing this jumper will cause the J-link reset to be high always, considering this point and placing J23 (pin 2-3) will cause VLDO to be cut from the daughterboard.

../_images/warning_j8.svg

Figure 13 J8 Jumper Placement

4.5. Connecting the DEVKIT-P to the Host PC

The DEVKIT-P Motherboard comprises essential components for seamless development:

FTDI Chipset U12: This chipset, represented by the FT2232HL, plays a crucial role in facilitating USB communication with the development host. It serves as a USB to UART bridge, establishing a seamless connection between the PC and the DA14533 SoC UART port. Additionally, it interfaces with the current sense circuitry through an SPI connection with ADC U8.

Power Supply (U5): U5 is responsible for providing a stable 3.3 V supply to power the FT2232HL chipset, ensuring its proper operation. Iti s worth noting that the chipset’s functionality relies on the presence of a 12 MHz crystal (Y1).

Embedded J-Link Debugger U25 (RA4M2): The embedded J-Link debugger, U25, is a valuable tool for debugging your development projects. It operates on a 3.3 V power supply from U5 and is enabled by the PWR_ENABLE signal.

Before connecting your ProDev Kit to the host PC, ensure that you have established the correct connections between the motherboard and your chosen daughterboard module. You have the flexibility to power the kit using either 3.3 V via USB (USB1) or VDD (a coin cell). When using a mini-USB cable, there is no need for an additional battery. To establish a connection, simply attach a standard mini-USB cable to the USB1 connector. For visual reference, see Figure 14.

../_images/connect_535.svg

Figure 14 DA1453x DEVKIT-P connections