10. Debugging via Serial Port
Enabling UART provides a convenient way to output diverse debugging information to a terminal emulator application. In this section, we’ll demonstrate how to activate UART for seamless debugging.
10.1. Serial Port Terminal
In the following we will demonstrate this using a standard and free terminal emulator, Tera Term but you can use any terminal emulator that you are comfortable with (PuTTY, RealTerm or else).
- First, we will set up Tera Term by selecting the virtual COM port and set the port configuration in the Setup->Serial Port window as shown below:
Figure 15 Tera Term, serial port settings
Click ‘OK’ to accept the port settings
Tera Term
Tera Term can be downloaded from https://osdn.net/projects/ttssh2/releases/
10.2. Enabling Serial Port
At this juncture, you can effortlessly enable UART by making a simple modification to the configuration file: …_config_basic.h Choose the appropriate file based on your desired target (User configuration modules).
- Scroll down and find the
#undef CFG_PRINTFstatement and change it to: - #undef CFG_PRINTF + #define CFG_PRINTF
- Scroll down and find the
In user_periph_setup.h change the gpio used as the UART transmit output by the DA14531 or DA1453x DevkitP and USB to
P0_5as follows:// Define UART2 Tx Pad #if defined (__DA14531__) #define UART2_TX_PORT GPIO_PORT_0 #define UART2_TX_PIN GPIO_PIN_5 #else #define UART2_TX_PORT GPIO_PORT_0 #define UART2_TX_PIN GPIO_PIN_4 #endif
This will automatically select and configure the proper GPIO for the UART TX. In order to give ourselves access to a more user friendly API, we will add the following include statement to user_empty_peripheral_template.c:
#include "arch_console.h"
- We can now use the following functions:
arch_puts(), to transmit a simple string via the UARTarch_printf(), to format and transmit a string via the UART
10.3. Using the Serial Port:
In our timer function,
my_timer_cb(), from the previous section of this tutorial, add the following statement:arch_puts("Turning the LED off after 2 seconds\n\r");
Build the project and load it onto target
Use your BLE explorer app to connect to the device and observe that the LED turns off 2 seconds after a BLE connection has been established while also transmitting
Turning the LED off after 2 secondsvia the UART:
Warning
The LED will not turn on if you are holding the button down while connecting!