7. General Purpose Output
- Controlling output ports on the Renesas SoC is pretty straight forward. It involves four steps:
Port and Pin Definition
Reservation of the pin
Configuration of the pin
Controlling the pin
7.1. Port and Pin Definition
- The Port and Pin definition specifies which physical pin is being used and is managed in the file user_periph_setup.h:
In user_periph_setup.h, we will define the LED on the development kit as
P1_0for the DA14585/6 variants andP0_9for the DA1453x:
#if defined (__DA14531__) #define LED_PORT GPIO_PORT_0 #define LED_PIN GPIO_PIN_9 #else #define LED_PORT GPIO_PORT_1 #define LED_PIN GPIO_PIN_0 #endif
Note
For DA14533 device, pins P0_6, P0_9 and P0_11 are not available
7.2. Reservation of the Pin
- In the
GPIO_reservations()function of user_periph_setup.c, we must reserve the port/pin pair for our LED as follows: RESERVE_GPIO(LED, LED_PORT, LED_PIN, PID_GPIO);
GPIO reservation
GPIO reservation ensures that we avoid conflicting usage of a port/pin pair during development.
7.3. Configuration of the Pin
Our purpose is to turn on the LED as result ,we must set the pin configuration in order to define it as a digital output.
- In
set_pad_functions()of user_periph_setup.c add the following line of code: GPIO_ConfigurePin(LED_PORT, LED_PIN, OUTPUT, PID_GPIO, false);
Note
The last argument is set false, indicating that we want the LED to be off initially.
7.4. Controlling the Pin
In order to demonstrate control of the general purpose output that we just created, we will use the LED to indicate BLE connection status. We will turn the LED on when the device is connected and turn it back off when the connection is terminated.
- In the file user_peripheral_template.c, add the following include statements at the top of the file:
#include "gpio.h" #include "user_periph_setup.h"
We will implement a function to turn on and off our LED. The function takes a boolean as an argument.When the argument is set to true, the function turns the LED on and when set to false it turns the LED off.
- In user_peripheral_template.c add this function right after the include statements:
void control_LED(bool state) { if(state == true) GPIO_SetActive(LED_PORT,LED_PIN); else GPIO_SetInactive(LED_PORT,LED_PIN); }
- The
user_on_connection()function will run whenever a BLE connection is established. We can turn the LED on in that function by adding a call to our new function: control_LED(true);
- The
- And in the
user_on_disconnect()we can turn the LED back off: control_LED(false);
- And in the
Build the project and load it onto your target
Now, use your BLE explorer app to verify that the LED on the development kit turns on and off to indicate the connection state
Note
If we enabled sleep mode at this point, we would observe an unexpected behavior. The LED would only light up for a very short period of time. This issue is explained and addressed in the Sleep Mode section of this tutorial