3. Figures
Figure 2 DA1470x Development Kit-PRO Setup
Figure 3 D/AVE 2D Block Diagram
Figure 6 Memory Layout Schemes
Figure 7 LCDC Color Conversion Scheme
Figure 8 Display Initialization Sequence Diagram
Figure 9 Display Update Sequence Diagram
Figure 10 Creating New Display Configuration File
Figure 11 Read Touch Event Sequence Diagram
Figure 12 LVGL Folder Structure
Figure 13 LVGL Color Conversion Scheme
Figure 15 DA1470x Development Kit-Pro
Figure 16 DA1470x Devkit-Pro Display and Touch Panel Connector
Figure 17 DA1470x Development Kit-Pro including AMOLED Display
Figure 18 DA1470x Development Kit-Pro - QUAD SPI Flash
Figure 20 Application List Interface
Figure 24 Application Objects, correlations and positions
Figure 26 1 Layer Sliding from the Watch Face to the Menu Screen
Figure 27 2 Layers Sliding from the Watch Face to the Menu Screen
4. Terms and Definitions
BLIT Block Image Transfer
CLUT Color Lookup Table
DBI-B Display Bus Interface Type B
DMA Direct Memory Access
DevKit Development Kit
DPI Display Parallel Interface
FB Frame Buffer
GDI Graphics Display Interface
GPU Graphics Processing Unit
JDI Japan Display Inc.
HW Hardware
I2C Inter-Integrated Circuit
LCD Liquid Crystal Display
LLD Low-Level Driver
LUT Look Up Table
LVGL Light and Versatile Graphics Library
PSRAM Pseudoptotic RAM
QSPI Quad Serial Peripheral Interface
RAM Random Access Memory
RGB Red Green Blue
RLE Run-Length Encoded
RTOS Real Time Operating System
SDK Software Development Kit
SoC System-on Chip
SPI Serial Peripheral Interface
SRAM System RAM
USB Universal Serial Bus
XIP FLASH Execute In Place Flash