UM-B-083 SmartSnippets™ Toolbox¶
Contents¶
- 1. Installation Guide
- 2. Getting Started
- 3. Programmer Operations
- 4. Estimator Operations
- 5. Manager Operations
- 6. Monitor Operations
- 6.1. Data Rate Monitor
- 6.2. Power Profiler
- 6.2.1. Supported devices, families and Power Management Module versions
- 6.2.2. Power Profiler Ribbon group
- 6.2.3. Chart controls and menus
- 6.2.4. Power Profile basic usage
- 6.2.5. Power Profiler software cursors
- 6.2.6. Power Profiler control panel
- 6.2.7. Power Profiler Chart Controls
- 6.2.8. Chart management via mouse
- 6.2.9. Chart management via keyboard
- 6.2.10. Power Profiler configuration
- 6.2.11. Calibration Procedure
- 6.2.12. Power Profiler special properties
- 6.3. Log
- 7. Configurator Operations
- 8. CLI implementation
- 9. Application Help
- 10. Troubleshooting
- 10.1. Error “2nd stage bootloader rejected (-105)” on Connect or Booter
- 10.2. Error message on not supporting ARMv8-M architecture
- 10.3. Warning on CLI interface running from windows: WARNING: Could not open/create prefs root node Software\JavaSoft\Prefs at root 0x80000002. Windows RegCreateKeyEx…
- 10.4. Firmware file in Hex format does not start running when downloading to the board
- 10.5. Error message during verification after erase or burn
- 10.6. Timeout error when working with large flash memory on JTAG
- 10.7. Flash Code / Flash Data : Content read is 0x00
- 11. Appendices
- 12. Disclaimers & Contact info