1. Abstract

This guide is intended to help customers setup the hardware development environment, install required software, download, and run an example application on the DA14585/586 Basic Development Kit development platform.

2. Prerequisites

  • Minimum hardware requirements:

    • Windows Operating System, 1 GHz, 32-bit or 64-bit processor

    • 1 GB of system memory (RAM)

    • 2 GB of available disk space

  • Basic Development Kit DA14585/586 and accessories

  • Serial-port terminal software (for example, Tera Term)

  • A USB connection supporting USB-Serial (FTDI)