2. Introduction
The purpose of this guide is to give an overview of the booting options available for the DA1453x family using the DA14531 or DA1453x DEVKT-P Motherboard. The BootROM Sequence will be executed when a POR or a HW Reset occurs or a RESET_ON_WAKEUP event happens which is a configurable feature. This document describes the available methods to connect, boot, and program the external Flash/EEPROM or the internal OTP. As this document is tailored for DA1453x family we recommend to take look at the following methods Datasheets.
The follwoing development kits comprises essential hardware, including a development board equipped with an on-board debugger. It is complemented by comprehensive support from a Software Development Kit (SDK6). This SDK includes a complete development toolchain, a rich collection of source code examples, and comprehensive documentation. Together, these resources provide developers with everything they need to kick-start their projects effectively and efficiently.
DA14531-00FXDEVKT-P
DA14535-00FXDEVKT-P
DA14533-00FXDEVKT-P