Using the EEPROM Programmer in SmartSnippets™ Toolbox you can download the image to the EEPROM memory and boot it from the EEPROM. The SDA and SCL lines to be selected in the board setup are P0_3 and P0_4 respectively.
The breakout for the 53x on the Motherboard would be P2_3 and P2_4, so connect the SDA and SCL to P2_3 and P2_4 using jumper cables.
Now click Connect and once connected select the firmware to download to the EEPROM memory.