1. Abstract
This guide is intended to help customers setup the hardware development environment, install required software, download and run an example application on the DA1459x development platform.
Note
DA1459x is referring to DA14592 and DA14594.
The below table presents the various members of the DA1459x product family and their supported features.
Features |
DA14592 |
DA14594 |
|---|---|---|
RAM capacity |
96 kB |
96 kB |
eFlash capacity |
256 kB |
256 kB |
Bluetooth® LE 5.2 core features |
YES |
YES |
Bluetooth® LE 5.3 core features |
NO |
YES |
Advertising Extensions support |
NO |
YES |
Periodic Advertising support |
NO |
YES |
AoA/ AoD support |
NO |
YES |
Wireless Ranging (WiRa) support |
NO |
YES |
Up to 32 GPIOs |
YES |
YES |
Packages |
WLCSP39 and FCQFN52 |
WLCSP39 and FCQFN52 |