Logo
  • ble_app_all_in_one crashes with hardfault when program DA14535 Module
  • ble_app_lecb L2CAP application can’t handle different src and dest cids
  • ble_app_lecb L2CAP L2CAP app does not reject with Insuff. Auth. when necessary.
  • ble_app_lecb L2CAP app does not add credits to its own channel
  • The DA14585 and DA14531-00 do not include the complete ‘SMP Timeout after Security Request’ fix.
  • syscntl_dcdc_turn_on_in_boost_ROM() leads to a hardfault when DA14531-01 and DA14535 configured in bypass mode
  • Driver configuration structures are not compatible with ROM functions on LLVM
  • Secondary bootloader may allow an unverified image to boot from UART
  • OTP write operation fails when using flash_programmer, jtag_programmer and secondary bootloader generated from SDK 6.0.24
  • Unexpected error assertion crashes SDK6 application
  • UART with DMA flow control
  • Improve error handling in case of AES issue
  • UART ROM driver: Not all baud rates are supported by the stack
  • Wrong register attributes allow modification of the device specific manufacturing data
  • Random number generator incorrectly seeded
  • DA14531 Temperature sensor driver in SDK
  • DA14531 prod_test otp_write function issue
  • DA14531 Trim value issue when waking up from hibernation with no ram retained
  • ADC interrupted with BLE activity
  • DA14585 Secondary Booter - Booting encrypted image bigger than 80KB
  • DA14531 IAR Example : Some missing configuration
  • SMP timeout caused by encryption request during SMP session
  • Always passing ATT_ERR_APP_ERROR in custs1_value_req_rsp_handler()
  • High temperature and RCX
  • PDM support
  • GLPS minor improvement
  • Weight Scale Service : Missing app-callback communication
  • DA14585/DA14586 Crystal trimming lost after sleep
  • Coexistence driver limits the pins for BLE_EIP from P00 up to P07
  • DA14531 ROM booter Limitations
  • I2C asynchronous slave reception
  • UART2 initialization infinite loop
  • Build error with PRODUCTION_DEBUG_OUTPUT enabled
  • HTPT Indication Problem
  • DA1453x bootROM boot specific configuration Limitation
  • Error in unused defines
  • Default system rand() function is not NIST compliant
  • HCI ACL fragmentation does not work correctly
  • Static Random BD Address calculation issue
  • Reset Indication characteristic not firing callback when status error is returned after first read
  • DA14531 Further secondary bootloader optimization for large image files
  • DA145x App_Easy_timer problem during long sleep time
  • Update XTAL32M settings to the robust settings as recommended in the HW guidelines
  • No GTL reply is sent to the host after a failed pairing attempt
  • SDK metric and RCX
  • DA14585 Peripheral does not generate GAPC_PARAM_UPDATED_IND
  • Secondary bootloader runs on both encrypted and un-encypted images
  • If during an SMP session the Master attempts to re-encrypt the link, the encryption request reaches the 531 Host after an SMP timeout is generated
  • ROM version of adc_input_shift_config() includes wrong delay
SDK6 Known Limitations List
  • Search


© Copyright 2026, Renesas Electronics Corporation.