No GTL reply is sent to the host after a failed pairing attempt
ID: LPCBARESDK-860
Status: Fixed
First reported: 6.0.16.1144
Fixed in: 6.0.20.1338
Description
The DA14531 and the DA14585/DA14586 devices don’t send a GTL packet to the external microcontroller informing it of the failed pairing during the phone connection.
Workaround
This is a ROM issue. It has been fixed in DA14531-01 ROM but not in the DA14585/586 and DA14531. For more details about the DA14531-01 device you can refer to the UM-B-117 and the DA14531 DataSheet.