ble_app_all_in_one crashes with hardfault when program DA14535 Module
ble_app_lecb L2CAP application can’t handle different src and dest cids
ble_app_lecb L2CAP L2CAP app does not reject with Insuff. Auth. when necessary.
ble_app_lecb L2CAP app does not add credits to its own channel
The DA14585 and DA14531-00 do not include the complete ‘SMP Timeout after Security Request’ fix.
syscntl_dcdc_turn_on_in_boost_ROM() leads to a hardfault when DA14531-01 and DA14535 configured in bypass mode
Driver configuration structures are not compatible with ROM functions on LLVM
Secondary bootloader may allow an unverified image to boot from UART
OTP write operation fails when using flash_programmer, jtag_programmer and secondary bootloader generated from SDK 6.0.24
Unexpected error assertion crashes SDK6 application
UART with DMA flow control
Improve error handling in case of AES issue
UART ROM driver: Not all baud rates are supported by the stack
Wrong register attributes allow modification of the device specific manufacturing data
Random number generator incorrectly seeded
DA14531 Temperature sensor driver in SDK
DA14531 prod_test otp_write function issue
DA14531 Trim value issue when waking up from hibernation with no ram retained
ADC interrupted with BLE activity
DA14585 Secondary Booter - Booting encrypted image bigger than 80KB
DA14531 IAR Example : Some missing configuration
SMP timeout caused by encryption request during SMP session
Always passing ATT_ERR_APP_ERROR in custs1_value_req_rsp_handler()
High temperature and RCX
PDM support
GLPS minor improvement
Weight Scale Service : Missing app-callback communication
DA14585/DA14586 Crystal trimming lost after sleep
Coexistence driver limits the pins for BLE_EIP from P00 up to P07
DA14531 ROM booter Limitations
I2C asynchronous slave reception
UART2 initialization infinite loop
Build error with PRODUCTION_DEBUG_OUTPUT enabled
HTPT Indication Problem
DA1453x bootROM boot specific configuration Limitation
Error in unused defines
Default system rand() function is not NIST compliant
HCI ACL fragmentation does not work correctly
Static Random BD Address calculation issue
Reset Indication characteristic not firing callback when status error is returned after first read
DA14531 Further secondary bootloader optimization for large image files
DA145x App_Easy_timer problem during long sleep time
Update XTAL32M settings to the robust settings as recommended in the HW guidelines
No GTL reply is sent to the host after a failed pairing attempt
SDK metric and RCX
DA14585 Peripheral does not generate GAPC_PARAM_UPDATED_IND
Secondary bootloader runs on both encrypted and un-encypted images
If during an SMP session the Master attempts to re-encrypt the link, the encryption request reaches the 531 Host after an SMP timeout is generated
ROM version of adc_input_shift_config() includes wrong delay
SDK6 Known Limitations List
Index
Index