5. Introduction

Based on the SmartBond DA14695 Bluetooth® low energy 5.2 system on chip (SoC), the DA14695MOD brings out all the DA14695 hardware features and capabilities, including a JEITA-compliant, USB Charger – ideal for rechargeable end products. The module integrates all passives, antenna, a 32Mbit QSPI FLASH and is supported by an easy-to-use software development suite.

For further reading More information can be found in the DA14695MOD Datasheet

The development kit includes a set of hardware (development board with an on-board debugger) and is supported by a Software Development Kit SDK (that is, a development toolchain, source code examples, and so on), and documentation.

5.1. Guide Purpose

The purpose of this guide is to provide an overview of the DA14695MOD ProDK and describe the setup of the hardware and installation of the software tools to fully use the module.

The guide is organized as follows:

  • Section 6 describes the hardware components and their initial installation and setup.

  • Section 7 and Section 8 describe the installation of the SmartSnippets™ DA14695 SDK software, along with all necessary tools.

  • Section 9 contains all steps for downloading and executing your first DA14695MOD application.

5.2. How long should it take?

This tutorial requires 10-15 minutes to complete. For more information the user may consult the accompanied documentation, these are mentioned as for further reading.

5.3. Ordering Information

The DA14695MOD ProDK (DA14695MOD-00DEVKT-P) can be ordered via various distributors.

For more information and purchasing please visit the DA14695MOD product page.

Customers should contact their distributor, representative or their field application engineer (FAE) for any support and Renesas is happy to help. Support is also available through the Renesas engineering community.