1. Abstract
This guide is intended to help customers setup getting started with the DA14695 Bluetooth® module Development Kit - Pro (DA14695MOD ProDK) from Renesas. The DA14695MOD is the:
Only Bluetooth® LE module in the market with built-in USB Charger which is ideal for rechargeable end-product applications.
Only Bluetooth® LE module in the market with display driver which is ideal for wearable applications or products with displays (eg connected medical, PoS Readers, etc).
2. Figures
Figure 1 The DA14695MOD Pinout Diagram
Figure 2 The DA14695MOD Daughterboard
Figure 3 The DA14695MOD Daughterboard bottom
Figure 4 The DA14695MOD connected to the DA14695 mother Board
Figure 5 DA14695MOD daughter board connection
Figure 8 Setting Up the Port and Testing connectivity via Tera Term
Figure 9 How to program the DA14695MOD with the standalone flash programmer tool
Figure 10 How to program the DA14695MOD with the SmartSnippets™ Toolbox
3. Tables
4. Prerequisites
To start evaluation or project development on Renesas DA14695 product sets – the following tools are recommended.
Hardware tools:
Computational workstation (e.g. PC or Laptop)
64-bit processor with 1 GHz processing speed
1 GB RAM
2 GB free disk space
DA1469x main board (DA14695MOD-00DEVKT-P) as a Motherboard.
DA14695MOD daughter board (DA14695MOD-00F1DB-P).
USB cable to power the Pro Development kit and perform on-board debugging
Software tools:
Terminal software such as RealTerm, Putty or Tera Term. This document uses Tera Term for its examples.
SmartSnippets™ Studio 2.0.20 or later which is available for Windows OS, Linux OS and macOS , see Section Section 8.
Bluetooth® LE explorer application because working with Bluetooth® requires access to some type of generic GATT explorer tool that supports features such as:
Scanning for Bluetooth® LE devices
Establishing Bluetooth® connection with a specific device
Discovering and interacting with GATT services
There are numerous options when it comes to GATT explorer tools. Until recently, these tools have mostly been supported via smartphone apps or through specific hardware connected to a PC. Recently, the Chrome Browser on Windows 10 and MAC books offer GATT exploration using the native Bluetooth® hardware on those platforms. Below is a subset of options:
Renesas Smartbond for IOS Use the QR code below
Renesas Smartbond for Android. Use the QR code below
Type chrome://bluetooth-internals/#devices into the address field of the Chrome Browser to use the built-in tool (PC with Win10 or MAC book)
Renesas SmartBond for iOS:
Renesas SmartBond for Android:
Note
When installing SmartSnippets™, all the sub-component drivers and software tools needed for DA14695 development will be installed.