11. Appendix B: SEGGER J-Link Firmware Update
The SEGGER J-Link onboard debugger that your Renesas DA14592 Devkit USB is equipped with, might request a firmware update. Please do the update prior to start working with your development kit.
To update your development kit’s SEGGER J-Link firmware, please follow the steps below.
Insert your Renesas DA14592 Devkit USB module in your PC USB port.
Execute the Renesas SmartBond™ Flash Programmer. Please always use the latest available version of the software.
Figure 37 Renesas SmartBond Flash Programmer
The Renesas SmartBond™ Flash Programmer detects your Renesas device and if any update is needed, it prompts you with a notification message, as is shown below. Please press Yes to update your firmware.
Figure 38 SEGGER J-Link Firmware Update Message
If the system succeeds to update your J-Link firmware, you will go to the initial Renesas SmartBond™ Flash Programmer screen, as is shown below. Everything is ready and you can use your Renesas kit.
Figure 39 SEGGER J-Link Firmware Update Succeeded
If the system fails to update your J-Link firmware, you will get a failure notification message as is shown below.
Figure 40 SEGGER J-Link Firmware Update Failed
In case your system fails to update your firmware, please close the Renesas SmartBond™ Flash Programmer software and execute the SEGGER J-Link Configurator software, as is shown below.
Figure 41 SEGGER J-Link Configurator
On your SEGGER J-Link Configurator software, please select the J-Link OB-SAM3U128 V3 USB connected device, as is shown in the image below, and click Update firmware of selected probes and programmers.
Figure 42 SEGGER J-Link Configurator Menu
You will get a confirmation notification if you want to update your firmware. Please press Yes.
Figure 43 SEGGER J-Link Configurator Updating Firmware
After successfully updating the firmware you will get a confirmation message in the Log section of the SEGGER J-Link Configuration software (marked in green), as is shown below. Also please check that your Host and Probe / Programmer versions match (marked in red).
Figure 44 SEGGER J-Link Configurator Updating Firmware Succeeded
Congratulations, you have successfully updated your Renesas DA14592 Devkit USB SEGGER firmware. Now you can use your kit.