Renesas e²Studio is the Integrated Development Environment for Renesas embedded microcontrollers.
e²studio is based on the industry-standard open-source Eclipse IDE framework and the C/C++ Development
Tooling (CDT) project, covering build (editor, compiler, and linker control) and debug phases with an extended
GNU Debug (GDB) interface support.
All Renesas BLE Development boards have an on-board J-Link debugger from SEGGER. This offers standard debug capabilities
such as single stepping, setting breakpoints, software download and many more. For more details on the debugger capabilities, visit https://www.segger.com/.
Hardware Environment:
Processor: x64-based processor, at least 2GHz (support hyper-threading/multi-core CPU)
Main Memory: At least 4GB, recommended 8GB of free memory space.
Hard disk Capacity: At least 2GB of free space
Display: Resolution at least 1,024 x 768; at least 65,536 colors
Interface: USB 2.0 (High-speed/Full-speed). High-speed is recommended.
Windows
Linux
Supported OS: Windows 10 and Windows 11 (64-bit edition).
In the Additional Software page, select the GNU ARM Embedded 7.2.2017q4 to be installed, then
click Next. This page is not shown if you selected Quick Install.
If you have already installed e²Studio without GCC 7 tools, then please download and install the GCC 7 tools
separately from github or simply re-install Renesas e²studio.
Tick the checkbox to accept the license agreement, then click Next to continue.
Installing… means the installation starts. Depending on the items selected in the “Addition Software” dialog, new dialogs may open to proceed with the installation of these software packages.
When the installation completes the Results page is shown. Click OK to proceed.
After the installation of the e²Studio completes, you need to install the Smartbond™ DA14592 SDK.
The Smartbond™ DA14592 SDK is used for application development using the DA14592 USB-DEVKIT or custom hardware including the DA14592 SOC.
The Smartbond™ DA14592 SDK includes a complete BLE Framework with a set of libraries, drivers, middleware modules and example projects
which facilitate the creation of complex applications by fully exploiting the provided hardware resources of the connected DA14592 device.
The Smartbond™ DA14592 SDK is based on the FreeRTOS operation system and supports execution-in-place (XIP) from internal eFLASH or external QSPI FLASH.
The Smartbond™ DA14592 SDK can be downloaded from Renesas’ Website
and installed on your PC at any convenient location.
The SmartSnippets™ Toolbox, Figure 17, is focused on enabling the process of programming eFLASH and optimizing code
for optimal power performance by allowing:
The re-programming of the eFlash with the actual application compiled image.
The seamless download and execution of a certain software image to RAM over UART.
Figure 17 SmartSnippets™ Toolbox : Various Mode Views
SmartSnippets™ Toolbox is also supported by other utilities such as the
Command Line Interface (CLI) Programmer. The CLI Programmer is a command
line tool for programming the DA14592 family of devices. It allows
erasing and programming the device eFLASH memory. This tool may be
used both in development and on the production line. The CLI Programmer
will be installed as an integrated part of the Smartbond™ DA14592 SDK.