5. DA14592 – USB-DEVKIT hardware
The USB-DEVKIT consists of a board featuring the DA14592 SoC, USB connector and a mikroBUS slot. More details about the DA14592 product family can be found in the DA14592 Datasheet.
5.1. The USB-DEVKIT board
Figure 1 illustrates the physical layout of the USB Development Kit.
- The USB-DEVKIT provides all necessary hardware to enable:
Full functional verification of the DA14592.
Full digital connectivity with external hardware using UART, SPI and I2C.
USB-based debugging capabilities using the SEGGER J-Link on-board debugger for Cortex M33 processor.
USB-based UART communication with the host PC using a Future Technology Devices International (FTDI FT2232H) chipset which converts UART to USB.
Figure 1 The DA14592 USB-DEVKIT
Notes
Some GPIO’s are routed to the MikroBUS connecter and can be used for monitoring GPIO and power signals.
The schematic diagrams, BOM, and Gerber files are illustrated in detail in the Development Kit Documentation.