3. Analyzing the Key Points of a Sample Code
This section covers the fundamental code structure found in every demonstration application included in Renesas’ SDK. All applications are implemented as FreeRTOS
tasks that are created under the system_init() routine.
3.1. The Key Points of the Main Function
The main() function is the basic routine of every source code and is responsible for the following actions:
To create the
system_init()task which is responsible for initializing the system. In this task all application tasks are being created as well.To trigger the FreeRTOS scheduler which is responsible for controlling and executing all the RTOS tasks, according to their priorities.
3.2. The Key Points of the System Initialization Function
System clocks should be initialised according to applications’ needs. The system clock, low power clock source, clock divider for the AMBA peripheral bus clock (APB) and AMBA high speed bus (AHB) should be set. The low power clock (lp) used is selected via
dg_configUSE_LP_CLKdeclared inconfig/custom_config_xxx.hfile. Valid values of this macro are:
LP_CLK_RCXused for selecting the internal RC oscillator.
LP_CLK_32768used for selecting the external crystal XTAL32K
LP_LCK_32000used for clocking the device using digital clocks generated either by another MCU or digital clock generator.Note
Since the WLCSP39 package has a limited amount of ‘pins’ the XTAL32K connections are not available.
By default, the code examples found in Renesas’ DA1459x SDK make use of the internal RCX oscillator as LP clock.
/*
* Prepare clocks. Note: cm_cpu_clk_set() and cm_sys_clk_set() can only be called from a
* task since they will suspend the task until the XTAL32M has settled and the PLL maybe
* locked.
*/
cm_sys_clk_init(sysclk_XTAL32M);
cm_apb_set_clock_divider(apb_div1);
cm_ahb_set_clock_divider(ahb_div1);
cm_lp_clk_init();
If
XTAL32Kis selected as low power clock, the system is prevented from entering sleep for approx. 8 seconds after a HW reset (cold boot). This delay ensures the external crystal is settled before the device utilizes it. After the passage of that delay, the device can enter sleep mode. Note thatsysclk_LPcannot be used as clock source while the device is active (system clock).
The next step is the initialization of the peripherals used by the target application. User should add their own functionality in
prvSetupHardware()routine.Select the preferred sleep as well as wakeup mode.
/*
* Upon a wakeup cycle, wait for the XTAL32M crystal to settle.
* BLE, USB and UART blocks require the XTAL32M to be up and
* running to work properly.
*/
pm_set_wakeup_mode(true);
/* Set the desired sleep mode. */
pm_sleep_mode_set(pm_mode_extended_sleep);
/* Set the desired wakeup mode. */
pm_set_sys_wakeup_mode(pm_sys_wakeup_mode_normal);
Figure 13 Possible Device’s States
After all system configurations is done, the application tasks should be declared.
Note
The last code line in system_init(), OS_TASK_DELETE(OS_GET_CURRENT_TASK()), is used for deleting the task itself. This is done in
order to release valuable system resources. After all, the initialization of the system only needs to be done once at beginning of device’s start.