1. Introduction
1.1. Before You Start
Before you start you need to:
Install the latest e² studio v2025-01 or later
Download the latest SDK for the DA1459x platforms, this can be downloaded from the DA14592 product page or DA14594 product page.
Additionally, for this tutorial a DA14592 Pro Development kit or DA14594 Pro Development kit is required.
The key goals of this tutorial are to:
Start working with a customized project
Analyze the key points of the code structure
Prepare both hardware and software to run a demonstration code example
Note
DA1459x is referring to DA14592 and DA14594.
The below table presents the various members of the DA1459x product family and their supported features.
Features |
DA14592 |
DA14594 |
|---|---|---|
RAM capacity |
96 kB |
96 kB |
eFlash capacity |
256 kB |
256 kB |
Bluetooth® LE 5.2 core features |
YES |
YES |
Bluetooth® LE 5.3 core features |
NO |
YES |
Advertising Extensions support |
NO |
YES |
Periodic Advertising support |
NO |
YES |
AoA/ AoD support |
NO |
YES |
Wireless Ranging (WiRa) support |
NO |
YES |
Up to 32 GPIOs |
YES |
YES |
Packages |
WLCSP39 and FCQFN52 |
WLCSP39 and FCQFN52 |