7. Debugging using printf
It is quite convenient to be able to output various debugging information via a serial port to a terminal emulator application. In this section we will demonstrate how to enable the serial port for this purpose.
7.1. Serial Port Terminal
In the following we will demonstrate this using a standard and free terminal emulator, Tera Term. Tera Term can be downloaded from Tera Term, but you can use any terminal emulator that you are comfortable with (PuTTY, RealTerm, +++)
First, we will set up Tera Term by selecting the virtual COM port and set the port configuration in the Setup->Serial Port window as shown below:
Figure 5 Set the serial port to 115k2/8/1/n as shown above.
7.2. Enabling printf
To enable printf via the serial port, we must again open the custom configuration file \config\custom_config_eflash.h, and add the following define:
#define CONFIG_RETARGET (1)
We must also add the following include in main.c:
#include <stdio.h>
At this point, we will be able to use printf in our project. We will modify the connection and disconnection handler to output the connection status.
In main.c find the connection event handler: handle_evt_gap_connected() and modify it as shown below:
static void handle_evt_gap_connected(ble_evt_gap_connected_t *evt)
{
printf("BLE Connection established: %d \n\r", evt->conn_idx);
}
Similarly, we will modify the disconnection event handler: handle_evt_gap_disconnected():
static void handle_evt_gap_disconnected(ble_evt_gap_disconnected_t *evt)
{
printf("BLE Connection terminated: %d \n\r", evt->conn_idx);
// Restart advertising
ble_gap_adv_start(GAP_CONN_MODE_UNDIRECTED);
}
Using the SmartBond™ Scanner smartphone app and Tera Term (or any similar terminal emulator), we can verify that our printf statements displays the BLE connection and disconnection events:
Figure 6 Tera Term output.