1. Abstract
This tutorial aims to provide a quick introduction to the Renesas SmartBond™ SDK10, while simultaneously demonstrating how to implement some basic functionality. The hope is that this tutorial will help users quickly understand the SDK structure and foundational concepts.
The tutorial uses a sample application in the SDK as a starting point and expands this application step by step. It is recommended that you follow along, but you should be able to select a specific topic from the index and manage to consume the tutorial in a piecemeal fashion.
The Renesas SDK10 supports the following SmartBond™ families:
Note
DA1459x is referring to DA14592 and DA14594.
The below table presents the various members of the DA1459x product family and their supported features.
Features |
DA14592 |
DA14594 |
|---|---|---|
RAM capacity |
96 kB |
96 kB |
eFlash capacity |
256 kB |
256 kB |
Bluetooth® LE 5.2 core features |
YES |
YES |
Bluetooth® LE 5.3 core features |
NO |
YES |
Advertising Extensions support |
NO |
YES |
Periodic Advertising support |
NO |
YES |
AoA/ AoD support |
NO |
YES |
Wireless Ranging (WiRa) support |
NO |
YES |
Up to 32 GPIOs |
YES |
YES |
Packages |
WLCSP39 and FCQFN52 |
WLCSP39 and FCQFN52 |